eo_logo
 
Product added to cart
 

Optical Filter Manufacturing: Products

products
 
PRODUCTS

Expertise and state-of-the-art equipment

Edmund Optics manufactures a wide variety of optical filters including bandpass, multi-bandpass, shortpass, longpass, dichroic, notch, and more! Not sure what kind of filter you need? Check out our filter selection guiede below and chat to one of our experts!

 
 

What We Can Make for You

Bandpass Filters

Bandpass filters transmit light of a certain clearly defined wavelength range and block adjacent wavelengths.

Key Specifications
  • Centre Wavelength (CWL) is the wavelength at the centre of the passband.
  • Full Width at Half Maximum (FWHM) is the bandwidth at 50% of the maximum transmission.
  • Peak Transmission (%) - wavelength of maximum transmission.
Special Cases
  • Multiband pass filter - bandpass filters with more than one passband.
Bandpass Filters
Bandpass Filters

Shortpass Filters

Shortpass filters transmit wavelengths below a certain (cut-off) wavelength

Key Specifications
  • Shortpass filters' "Edge Steepness" or "Slope" specifications denote sharpness of transition between transmission and adjacent blocking band; given as distance (nm) or percentage (%) of the edge wavelength (cut-off or cut-on respectively).
  • At Edmund Optics, it is the distance from the 10% to the 80% transmission point.
  • Example: A 500nm longpass filter with 1% slope has a transition over 5nm bandwidth (1% of 500nm) from 10 – 80% transmission.
Shortpass Filters
Shortpass Filters

Longpass Filters

Longpass filters transmit wavelengths above a certain (cut-on) wavelength.

Key Specifications
  • Longpass filters' "Edge Steepness" or "Slope" denote the sharpness of transition between transmission and adjacent blocking band; given as distance (nm) or percentage (%) of the edge wavelength (cut-off or cut-on respectively).
  • At Edmund Optics, it is the distance from the 10% to the 80% transmission point.
  • Example: A 500nm longpass filter with 1% slope has a transition over 5nm bandwidth (1% of 500nm) from 10 – 80% transmission.
Longpass Filters
Longpass Filters

Notch Filters

Notch filters block light of a certain clearly defined wavelength range and transmit adjacent wavelengths.

Key Specifications
  • Also called "Band Stop" or "Band Reject Filters".
  • Their blocking band (or stopband) is the spectral band that is blocked, often a laser line.
  • Blocking may be achieved by absorption or reflection.
  • Rugate coating designs can be very effective for reflective notch filters.
Notch Filters
Notch Filters

Dichroic Filters

Dichroic filters separate a broad spectral range into two components, a reflected and a transmitted component.

Key Specifications
  • Also known as "Dichroic Mirrors" or "Beamsplitters".
  • Note: "Dchroic Filters" is also sometimes used for referring to interference filters.
  • Often designed for 45° AOI.
  • Commonly used to separate excitation source and emitted fluorescence in fluorescence applications.
  • Longpass or shortpass dichroic designs possible.
Dichroic Filters
Dichroic Filters

Multi-Bandpass Filters

Multi-Bandpass Filters

Segmented RGB Filter

Segmented RGB Filters

Colour Glass Filters

Segmented RGB Filters

 Need small quantities fast?

Shop Edmund Optics® Marketplace for the world’s largest selection of off-the-shelf optical components with same-day shipping.

Colour Glass Filter Pricing Tool

Quoting for custom sizes.

Get Quote
 
 

Glossary

FAQ  Bandpass
Also referred to as waveband, passband, or bandwidth, bandpass is the wavelength range used to denote a specific part of the spectrum that passes incident energy through a filter. The first order is always at the design wavelength of the filter.
FAQ  Blocking
The blocking amount is the amount of light that is rejected, not passed, by a filter outside the passband. It is expressed as the ratio of total energy transmitted outside the passband to the total energy transmitted within the passband. Blocking values are given over a specified wavelength range.
FAQ  Blocking Range
Also referred to as the stopband, blocking range is a wavelength range used to specify a spectral region of energy that is not transmitted by a filter. It is typically specified in terms of Optical Density (OD).
FAQ  Central Wavelength (CWL)
Used to denote the peak transmitting wavelength of a filter, it is the midpoint determined by the passband wavelengths where the transmittance is 50% of the peak (denoted by the Full-Width at Half Maximum).
FAQ  Cut-Off Wavelength
Cut-off wavelength is the wavelength at which transmission decreases to 50% in a shortpass filter.
FAQ  Cut-On Wavelength

In filter terminology, cut-on is the wavelength at which the transmission increases to 50% throughput in a longpass filter.

FAQ  Filter
Filters are optical components that transmit, reflect, or absorb certain wavelengths or frequencies of light. Filter types include bandpass, longpass, shortpass, interference notch and rugate notch, color, dichroic, and neutral density.
FAQ  Full Width at Half Maximum (FWHM)

A specific wavelength region of the bandwidth of a filter defined by the two points of the passband where transmittance is 50% of the peak.

FAQ  Longpass Filter

A type of filter in which the transmission band is a region of longer wavelengths as compared to the region blocked.

FAQ  Neutral Density Filter (ND)

A type of filter that yields a constant value for attenuation, or optical density, over a bandwidth (i.e. spectrally flat). It is useful for attenuating, or reducing, overall light in a system.

FAQ  Notch Filter

A type of filter designed to block a pre-selected bandwidth and transmitt all other wavelengths within the design range of the filter. Notch filters are manufactured using the dielectric stack method which involves using a series of thin layers of dielectric materials, of alternating refractive index.

FAQ  Optical Density (OD)

Optical density is a value that describes the amount of energy that can pass through an optical material. It is directly related to the transmittance of the material. The greater the OD, the more light being blocked.

FAQ  Peak Transmittance

The highest transmittance value for light being passed by a filter.

FAQ  Peak Wavelength

The wavelength of light that has the highest transmittance value.

FAQ  Reflection

Radiation that changes direction, but not wavelength, after contact with a material surface.

FAQ  Shortpass Filter

A type of filter where the transmission band is a wavelength range of shorter wavelengths, typically lower than the region blocked.

FAQ  Transmission

The amount of radiant energy that passes through an optical medium, not being absorbed, reflected, or scattered.

FAQ  Wavelength

The peak to peak distance covered by one cycle of an electromagnetic wave. It is inversely related to frequency. The longer the wavelength, the lower the frequency; conversely, the shorter the wavelength, the higher the frequency.

 
Edmund Optics logo

Servicing our customers through specialized solutions:

Marketplace

One-stop shop for
the best brands and products
in optics and photonics

Manufacturing Services

Custom and volume
manufacturer of quality optical and
imaging components and systems